12/16/2018 11:41 PM | |
Joined: 9/27/2006 Last visit: 3/29/2024 Posts: 12249 Rating: (2660) |
Hello Narove; Which S7-200 CPU are you using? Did you use the MicroWin Position Control Wizard to generate your PTO functions? It makes your life really easier, see the description in Chapter 9 of the S7-200 System Manual: https://support.industry.siemens.com/cs/ww/en/view/1109582 Every PTO instruction has an Error output that you can check when your blocks do not work as specified. the definition of the error codes are available as part of the manual suggested above. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on