12/18/2018 9:24 AM | |
Joined: 6/7/2018 Last visit: 9/18/2024 Posts: 3 Rating: (0) |
Hi, is there a way to generate a source from a SFC or SFC type? |
12/19/2018 8:06 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello U_a6a66ecf-f750-4b18-9937-409f64ec2c2e, what do you mean with generate source from a SFC or SFC Type? Normaly you click on menu command SFC > Compile.... and then the charts of the current program (chart folder) are checked for consistency and compiled. Each SFC in the chart folder is mapped as follows during compilation:
I don't know an other way to generate the blocks, because the compiler will also generate the additional blocks that are used for executed the SFC or SFC-Type in the AS. You can find an overview of the blocks generated during compilation here. With regards |
Follow us on