4/9/2015 2:58 PM | |
Joined: 11/25/2013 Last visit: 9/16/2024 Posts: 35 Rating: (0) |
Dear Sir I get vector fault (External Fault 1(F07860)) at drive CU320-G130 and I get this fault when the drive at off mode and when the drive at running mode not appear. Regards ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/10/2015 11:09:41 AMNew subject after splitting |
|
5/29/2016 9:12 AM | |
Posts: 1 Rating: (0) |
What are the remidies of fault F07860 .If problem is in the CU320 . How to by pass or clear. |
12/19/2018 1:37 PM | |
Joined: 5/30/2012 Last visit: 10/22/2023 Posts: 1 Rating: (0) |
Put the value "1" in P2160. If you use Starter or TIA it is among the choices. |
Follow us on