3/21/2018 10:18 AM | |
Posts: 7 Rating: (0) |
ChristopD have you got an idea to solve this cause i havent fond a solution |
3/21/2018 3:11 PM | |
Joined: 7/9/2015 Last visit: 4/23/2024 Posts: 3809 Rating: (554) |
Hi, please check if local service are running: - S7 Dos Help Service or Simatic IEPG Help Service - also check this FAQ - yes it´s for connecting to real PLCs but can help also with PLCSim How can you set up the online connection again between the PG and the CPU?Also check this FAQ - yes it´s for connecting to real PLCs but can help also with PLCSim How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible?Regards, Towome |
|
|
12/30/2018 8:46 AM | |
Joined: 1/14/2018 Last visit: 2/28/2024 Posts: 9 Rating: (1) |
hi use the plcsim MPI , then go tho cpu and make connection them by use MPI connected |
7/13/2022 8:25 PM | |
Joined: 7/12/2022 Last visit: 7/14/2022 Posts: 1 Rating: (0) |
Thank you. It worked for me! |
Follow us on