12/28/2018 5:12 PM | |
Joined: 3/14/2008 Last visit: 3/28/2024 Posts: 2059 Rating: (924)
|
Hi, Can you try running OS project editor on the computer again? |
If I could help you, you can use the RATE button. Thank you. |
|
12/29/2018 6:07 AM | |
Joined: 9/15/2015 Last visit: 12/7/2022 Posts: 67 Rating: (6) |
Hi, Which settings should be concerned? I tried to open in other computer and it worked fine. :| only my computer... |
12/29/2018 1:27 PM | |
Joined: 3/14/2008 Last visit: 3/28/2024 Posts: 2059 Rating: (924)
|
Hi, The OS Project Editor must be set for each PC station. It will set the correct layout of screens, alarm settings and pictures/scripts. I suggest you disable everything in the print screen, except screens starting with @sfc, if you check them, you will receive the files from the installation directory. Maybe some of the faceplates are corrupted or changed...so running OS project editor will restore files |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on