1/16/2019 7:15 PM | |
Joined: 3/2/2015 Last visit: 5/11/2024 Posts: 63 Rating: (2) |
Hi, I have been stuck with this problem since last two days. Project involves CPU319F connected to a number of PN and PB nodes, and WinCC Flexible RT. I am trying to configure Report System Error, as far as configuration through Simatic Manager of RSE goes, it completes and FB49 and related blocks are generated and downloaded to PLC. In RSE Configuration I haven't checked the HMI Diag DB125/126 because when enabled it overwrites the DB126 used by FB126 PNIO Diag. Through CPU Messages tool, I am also able to see the messages. But within WinCC Alarm window nothing appears. Normal project alarms that were configured do appear but RSE alarms are not visible at all. I have gone through FAQ and configured the Alarm procedure, as well as Alarm Window and connection. Also I do not see any texts matching the RSE messages in Project Texts. I have tried deleting temporary files, separating the project from Simatic Manager and reintegrating back, compiling after RSE configuration, Rebuild All, Reconnect, Save with Optimization, Save with Reorganization (Slow) with no luck so far. Don't know what I am missing here. Kindly help. Regards, Anas |
Last edited by: Jen_Moderator at: 1/17/2019 11:36:06 AMOptimized link. |
|
Follow us on