3/30/2016 6:16 AM | |
Posts: 21 Rating: (0) |
in my system s7 300 the cpu is showing SF fault but in the IM module are ok . then what is the solution? |
6/27/2016 4:23 PM | |
Joined: 10/5/2015 Last visit: 4/23/2024 Posts: 1 Rating: (0) |
Hi guys, I have the same problem with random SF LED on CPU 315 2 DP. System worked flawlessly for 10 years and now starts to fail. We have checked power supply (replace with new one), replace all DO cards, replace IM365, replace CPU and the problem won't let go. If someone have an idea, we are here to listen. Thank you in advance. AttachmentVollert1.txt (798 Downloads) |
5/9/2017 4:14 PM | |
Posts: 1 Rating: (0) |
Hi, Can i know which I/P linked with which O/P. |
9/5/2018 6:48 PM | |
Posts: 1 Rating: (0) |
Please help, I tried MRES, clear/reset, power cycle and problem still there. BF2 LED blinking and SF is solid red.
AttachmentDiagnose.txt (674 Downloads) |
9/6/2018 2:51 AM | |
Posts: 14 Rating: (0) |
I also get this red light error once after placing an analog IM. What i did was, see pic. and problem solved |
Follow us on