2/13/2019 2:13 PM | |
Posts: 2 Rating: (0) |
The problem looks like mine.......can get the td10 working with the s5-95u........is there an manual for the td10..... how to get it working ??? my system just fel without power.......now the plc works again, but the td10 says ''READY FOR TRANSFER .'' What schould i do .....? greetings André ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/14/2019 7:37:13 AMNew subject after splitting |
|
2/13/2019 3:15 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Dré; Here is the only link I have found fr the TD 10 manual; it is from a streaming site you must register to, in order to download it. Siemens does not keep this old archive anymore. https://docs.google.com/document/d/1rfa-gzirn54FhJSJfBz5f9A5O_kArS0EXSkTehKitWY/edit The programming software for this Text Display was ComText, and it was used to connect to S5 CPUs through a RS-232 to TTY converter cable (6ES5734-2BD20, I believe), However, if all you want to know is how to upload the program in the TD 20, the answer is very simple: you can't. These units had very little memory, and all that was downloaded to them was a compiled version of the program, which you cannot disassemble even if you could upload it. See the following discussion from outside the Siemens forum for more insights; https://control.com/thread/1026167180 Hope this helps, Daniel Chartier |
Follow us on