2/7/2019 7:40 PM | |
Joined: 6/1/2017 Last visit: 5/8/2024 Posts: 13 Rating: (0) |
Dear friends I am using AI8 X 12bit 6ES7 331-7KF02-0AB00 module and my analog input is 0-10V but in HW configuration I can't find 0-10v . There are -+ 10 , -+5, -+1 v, not a 0-10 v Help me plzzz as soon as ------------------------------------------------------------------------------------------ |
Last edited by: Hafiz fiaz at: 2/7/2019 7:45:55 PMLast edited by: Jen_Moderator at: 2/8/2019 6:38:12 AMNew subject after splitting |
|
2/7/2019 9:11 PM | |
Posts: 2826 Rating: (685) |
There is no problem for you. Set the hardware to use the range [-10 .. 10] V. You will use only the (+) part of the range. Earlier in this topic (1st reply) is mentioned the posting that you should read slowly Your case use only internal value 0 to +27648. Forum note .. please do not post more than one of the same question. It would be most welcome if you deleted the other 3 questions. |
This contribution was helpful to1 thankful Users |
2/8/2019 6:34 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33792 Rating: (4197) |
Take a look at this Siemens FAQ |
Follow us on