1/23/2019 12:19 PM | |
Joined: 10/10/2014 Last visit: 4/18/2024 Posts: 1725 Rating: (209) |
Hi Evry If i see correct you use PCS7 faceplates. Move your pots to PCS7 part Best regards schufri |
1/23/2019 12:26 PM | |
Posts: 6 Rating: (0) |
Hi schufri. thanks for the answer how to do it ? |
1/28/2019 12:26 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Evry, to show an additional faceplate (MonAnL) in the another faceplatte (MotL) you have to connect any output from the MonAnL-block to the input "SelFp1" from the "MotL"-block. It is irrelevant if the block icon from MonAnL is created. More information you can find in the manual SIMATIC Process Control System PCS 7 Advanced Process Library at section Opening additional faceplates. With regards |
2/10/2019 5:56 AM | |
Posts: 6 Rating: (0) |
Hello Heisenberg. Yes, I did it. On ES everything works as it should. |
2/14/2019 4:55 PM | |
Joined: 11/10/2010 Last visit: 4/25/2024 Posts: 165 Rating: (8) |
hey, are you sure you did compilation of the OS before Downloading it ? Best regards |
2/15/2019 2:46 AM | |
Posts: 6 Rating: (0) |
hi. Yes, compile OS from step7. Without compilation, it did not work for the ES, and only works for the ES, OS - no. Best Regards |
Follow us on