2/26/2019 1:17 PM | |
Joined: 10/29/2014 Last visit: 12/18/2023 Posts: 7 Rating: (0) |
Hello!! I have a similar problem..I have a WinCC V7.4 SP1 upd4 project and i am connecting with OPC DA to a Telecontrol Server Basic (TCSB V3.1) OPC Server. The connection is establishing correct but i have many disconnections for 5 minutes. I have made the DCOM settings as described in the https://support.industry.siemens.com/cs/ww/en/view/109483815, but the problem is still there. The WinCC and the TCSB are running in the same machine. Here is some diagnose entries from project : 2303,26.02.2019,13:13:06:215,1000204,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' disconnected,MSG_STATE_COME 2303,26.02.2019,13:17:42:978,1000204,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' connected,MSG_STATE_GO 2303,26.02.2019,13:17:42:978,1000205,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' connected,MSG_STATE_COME 2303,26.02.2019,13:39:03:058,1000204,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' disconnected,MSG_STATE_COME 2303,26.02.2019,13:43:34:846,1000204,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' connected,MSG_STATE_GO 2303,26.02.2019,13:43:34:846,1000205,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' connected,MSG_STATE_COME 2303,26.02.2019,13:44:19:792,1000204,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' disconnected,MSG_STATE_COME 2303,26.02.2019,13:48:56:583,1000204,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' connected,MSG_STATE_GO 2303,26.02.2019,13:48:56:583,1000205,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' connected,MSG_STATE_COME 2303,26.02.2019,14:10:58:526,1000204,4,,SRV1,DataManager Runtime,TSDD7 Connection 'TSDD7' disconnected,MSG_STATE_COME Thanks a lot... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/27/2019 9:40:54 AMNew subject after splitting |
|
Follow us on