2/24/2019 7:05 AM | |
Joined: 8/19/2017 Last visit: 4/24/2024 Posts: 79 Rating: (3) |
Is there any way to update the nested charts that has been used in program just like updating blocks? |
2/27/2019 10:09 AM | |
Joined: 8/19/2017 Last visit: 4/24/2024 Posts: 79 Rating: (3) |
Hello Heisenberg2 I don't want to update blocks inside the nested chart. I want to create a chart and use it multiple times. It is possible that I make some changes in the mother chart, is it possible to update automatically all of the used charts after I made changes to the mother chart? Thanks in advance. |
2/27/2019 10:38 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Soroosh.v,
in this case I don't know any workaround to update automatically all of the used charts. The only way I know is with copy and paste the nested chart and drag&drop the connections. With CMT you can update all changes from an master type to all instance with an comfortable interface, but CMTs doesn't support chart-in-chart technology. With regards |
2/28/2019 9:34 AM | |
Joined: 11/10/2010 Last visit: 4/26/2024 Posts: 165 Rating: (8) |
hello, you must use CMT, control Modle Types in your charts, hope this doc can helps you
AttachmentCMT_Synchronisieren_en.pdf (239 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on