2/20/2019 1:25 PM | |
Posts: 39 Rating: (0) |
Hello everyone I have a problem with Wincc server. I have to create a server and three other users should have an access to this server. Now I have five PLC-s in the project (Siemens s7-1500) and I added to this project regular “PC station” with WinCC RT Prof. and “IE general” all this device are connected by one common PROFINET. Currently I using Wincc as below: I have all graphics and tags on screens in WinnCC prof. and i select this PC station and I click: Online > Download to file system, all files are created in folder. File with type “mcx” I’m using by “WinCC Runtime Start” and everything works. It is correctly way to using it ?How I shout connectother users? When I want to download PC station with Wincc prof.(server) on PC I have that error : “Check whether the SCS network adapter of engineering station is configured and enabled” . Next question is about clients How I shout download files to selected PC by network or can I do it by portable device ? I don’t have opportunity to use “Download to device” in PC station with clients ? Thanks |
Last edited by: morylATCS at: 2/20/2019 1:26:26 PM |
|
2/28/2019 7:04 AM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating: (68) |
Hello morylATCS, I found a forum discussion which partly is about the error message you've got:
I link it here for you and hope this is helpful: Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
2/28/2019 1:34 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1645)
|
Hello in winCC TIA Portal you do not have Clients with own Project (yet) like in WinCC v7.X. so you use only a Remote Open of the Serverproject on the Client. All you have to know is written in TIA Portal Help System at: Visualise Processes-> Options -> WinCC Server or in : https://support.industry.siemens.com/cs/de/en/view/109764577/105095184523 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on