2/22/2019 3:41 PM | |
Joined: 11/2/2008 Last visit: 9/18/2024 Posts: 92 Rating: (1) |
Hello Siwarexi, I am also facing same problem with WP231 i.e. when I am doing auto calibration I am getting error 7007 My WP231 is integrated with S7-1215C CPU in pressing application. Load cell capacity 5000lbs i.e. 2268 Kg In a parameter current load cell signal (mV) DR31 I am getting -0.1mV for 1 load cell If I replace load cell with other one then I get -0.24mV Excitation voltage is showing 4.91V If I reverse the polarity of Sig+ and Sig- then I could finish calibration without error but then I get -ve value of weight. And value is also not proper i.e. we putting 11.4 Kg of weight then Its showing 17 Kg in Siwatool or PLC. Is there any way to adjust this manually. Thanks and Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/25/2019 12:29:59 PMNew subject after splitting |
|
Follow us on