3/6/2019 12:02 PM | |
Joined: 9/9/2015 Last visit: 5/9/2024 Posts: 727 Rating: (268) |
Hi OF, For APL, there are using structures for all linkings. Inside the structure, there is normally a value (BOOL, REAL, WORD) and a signal status (BYTE).. For example, structure "FbkRun" in VlvL, Inside the structure, there is a input called "Value" And "ST". They assigned S7_m_c to the value only. So there will be a tag called Chartname/Blockname.FbkRun#Value inside the wincc tag management. Then the tag is ready to be used in faceplate/HMI. For User data block, if you would like to add OCM, you need to define appropriate attribute and go to blocks view in component view, look for the DB, right click, special object properties, Operator control and monitoring, enable it. Hope this is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on