3/7/2019 9:36 AM | |
Joined: 5/14/2018 Last visit: 6/13/2024 Posts: 8 Rating: (0) |
Hi, I am having an issue with the communication between SIMIT and PCS7. I am using simit v10 and pcs7 v9 sp1. digital signal works fine, i.e. whatever i simulate in SIMIT, PCS7DI block gets the signal too. problem is with the analog signals, PCS7ANIN is not showing any changes corresponding to whatever values i have at the output signal in SIMIT. I have tried to connect the phys to raw and signed to unsigned into the output signal in SIMIT. but no changes. all analog signals are affected. Pls help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/7/2019 11:21:02 AMNew subject after splitting |
|
3/7/2019 11:22 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject SIMIT Analog simulation problem is published within the conference Process Control Systems SIMATIC PCS 7. Best regards Jen_Moderator |
Follow us on