5/8/2018 7:19 AM | |
Joined: 4/28/2015 Last visit: 10/9/2023 Posts: 394 Rating: (55)
|
Hello, as I know, the SINAMICS V90 is using telegram 105 to communicate with the controller. Maybe it is useful for you to use telegram 105 in your project too, instead of telegram 3 - if this is possible with SINAMICS S110... To get an overview over the telegrams of S7-1500, please have a look to the manual at chapter 3.2 "Basics - Axes" (page 36...) SIMATIC S7-1500 S7‑1500 Motion Control V4.0 in TIA Portal V15 |
3/15/2019 6:36 AM | |
Joined: 1/20/2010 Last visit: 8/3/2021 Posts: 5 Rating: (0) |
Hello, I hope so that you solve this problem. How you solve this problem? I have the same situation. Thanks in advance! |
Follow us on