3/16/2019 2:23 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Soroosh, Disclaimer, im not that sure, but let me try to answer. I think it should work as well. Did you install your version of library of pcs7An driver block? You will never be able to generate module drivers without library install as there are some files missing in the systems now. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/16/2019 3:39 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684) |
Hello Soroosh.v; The basic design of a PCS 7 AS is based on S7-400 CPUs. You cannot use a S7-300 CPU as an AS. You can integrate a S7-300 as a seperate staion in PCS 7, as a subsidiary system, but only if you use the IL (Industrial Library) for S7-300 and HMIs. But even with IL you cannot have the S7-300 as a main control station in PCS7. Have a look at this Application example for IL: https://support.industry.siemens.com/cs/ww/en/view/50708061 Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on