3/7/2019 5:28 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
Hi TO-220, The manual "PCS 7 Advanced Process Library (V9.0 SP2)" is very extensive. It explains every detail of every module: SIMATIC Process Control System PCS 7 Advanced Process Library (V9.0 SP2) A recommended document for operation / WinCC is the manual "Compendium Part D": Part D - Operation and Maintenance
|
SIMATIC PCS 7 - Overview |
|
3/13/2019 9:57 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello TO-220, I don't know an documentation for the APL scirpt functions. Only APL Style Guide descripts how to create your own block, blockicon and faceplatte. And there you can find some information about the APL scripts but not all. Why do you want to use these scpirt function? The APL offers standardized button, displays and lot of more to create your own faceplatte with APL functionality. You can find the buttons and displays in the @PCS7ElementsAPL.PDL. With regards |
3/18/2019 7:39 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello TO-220, In my opinion the failure is by WinCC and not by the APL. The operator messages will generated from WinCC (see the manual WinCC V7.4 SP1: Working with WinCC). There you also find a list that you have to consider when you want to use an operator message. With regards |
3/21/2019 12:57 PM | |
Joined: 1/24/2019 Last visit: 4/17/2024 Posts: 56 Rating: (0) |
Excellent! Thank you for that link. I havent had much time to look back into this yet, but I think it is a failure of WinCC as well. One forum post mentioned that similar symptoms appeared when upgrading versions and that a rebuild or something was needed on the client. Will have to look into that more. But in general, I would also like to find more information on scripting. It seems a little sparse. There are a few forum posts concerning scripting but most of the links referenced are dead. Check out the following forum post, all links are now dead. https://support.industry.siemens.com/tf/ww/en/posts/need-vbs-actions-examples/96902/?page=0&pageSize=10 |
3/21/2019 1:30 PM | |
Joined: 1/24/2019 Last visit: 4/17/2024 Posts: 56 Rating: (0) |
Bang Bang : ) Found a scripting manual: https://support.industry.siemens.com/cs/ww/en/view/109736230 Thank you all very much! |
Last edited by: Jen_Moderator at: 3/22/2019 9:27:05 AMOptimized link. |
|
This contribution was helpful to2 thankful Users |
Follow us on