3/25/2019 3:35 PM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728)
|
Hello If you do a delta download of your Project then only the enginieernig Data will be transfered and the Runtime Files are still present. But if you want to change the Folder and so on then you can only try to copy the old Data in your new Project. You can try to use this FAQ (its for the Classic world but it should also work with WinCC Professional) http://support.automation.siemens.com/WW/view/en/24193864 Or you copy the old Database segments in the common Archiving Folder then your old data segments will be loaded into runtime. But this could be only a temporary solution. Bye Murof Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on