3/30/2019 10:45 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
HI, Just a quick question I hope someone can answer in the sample project i have attached I have simulated the line speed using a pulse generator and a division in maths block b0024. the target is 75 shackles per min but the shackles are on trolleys so therefore that would be 150 trolleys in the minute(because not all trolleys have shackles attached).I am using trolleys to trigger pulse. is the logo able to cope with the frequency of the pulse because if I run the project in simulation mode the return figure does jump around a bit,is the norm and am I being to picky Regards Attachmentspeed_m_c_stops_line1_V4_test.zip (182 Downloads) |
3/30/2019 11:23 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Ok, Thank you. it might be time to look at a s7-1200 |
3/30/2019 11:49 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066)
|
Simulation is simulation and not the real world. Whether it works can only be a practical test with a real LOGO! demonstrate. Attachmentspeed_m_c_stops_line1_V5_test.zip (199 Downloads) |
Last edited by: ixo65 at: 3/30/2019 11:49:41 AM |
|
Follow us on