4/3/2019 6:50 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, Which Windows 7 build are you using? I can cross check this build with mine. Please check below link if you have installed a Microsoft patch which may not be used. It seems your Windows version is OK to use, I installed PCS7 at least 20 times on Windows 7 without any issues. Maybe you can reinstall Windows 7? and make sure updates are off Also follow the following manual, especially chapter 4: PC Configuration |
Last edited by: Oreca at: 4/3/2019 8:17:29 AMLast edited by: Oreca at: 4/3/2019 8:18:18 AMLast edited by: Jen_Moderator at: 4/3/2019 11:23:39 AMOptimized link. If I could help you, you can use the RATE button. Thank you. |
|
Follow us on