4/4/2019 9:27 AM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077) |
The "#" is the sign for a so-called connector. It is used to store binary intermediate results. At S5, only one assignment can be made per network segment. If you now need a part of the network segment as, this connector is used. In your case, this makes no sense, since the AND block before only the F51.2 has as input. So F51.1 has the same state as F51.2 AttachmentSTEP5 V7.2 manual page 132.pdf (140 Downloads) |
Last edited by: ixo65 at: 4/4/2019 9:31:53 AM |
|
4/4/2019 10:13 AM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077) |
Yes, without the connector you must use two segments.
AttachmentEditor.pdf (135 Downloads) |
Follow us on