3/29/2019 9:42 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello anatoly.v, before you can see the data in WinCC Explorer you have to compile the OS. With an OS compile all of the data from SIMATIC Manager, such as tags, messages and texts as well as the hardware and connection configurations are "made known" to the OS. But not all data from the SIMATIC Manager will be transfered to WinCC, so the DB with the attribute S7_m_c which isn't part of the CFC will not transfered to WinCC. With regards |
4/3/2019 12:12 PM | |
Joined: 11/13/2013 Last visit: 10/18/2023 Posts: 35 Rating: (0) |
Thank for reply.
* put all logic into the block, * shared all IN_OUT variables (S7_m_c attribute), * put the FB into CFC chart. |
Follow us on