4/5/2019 8:57 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (267) |
Dear anatoly.v, Let me try to assist too. 1. copy all the blocks (especially those blocks in the chart) from Lib to the Station project. Replace/override all of them. 2. go to the station, CFC editor-> Option -> block type-> clean up -> highlight all -> Clean And next -> highlight all -> Clean. 3. Again, go to Option -> block type -> Highlight all from the left -> press insert to the chart database. 4. compile again and check. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to5 thankful Users |
4/5/2019 9:24 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi anatoly.v, Your topics suggest you are a Step7 programmer working in a PCS7 project. Please bear mark that you must forget about DB's,FB's,FC's etc.. PCS7 drives on CFC programming language where you take blocks from CFC library and import them in CFC program. You can create your own blocks, for example SCL language. Compile the source as block and then importing the block in CFC program. Your CFC program must then be downloaded to the PLC and must remain consistent. Each change in CFC language must be downloaded to the PLC. What I want to suggest is that you take a look at the following manuals: This will show you the way on how to work with PCS7. Good luck and if you need further assist, please let us know! |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on