3/27/2019 7:30 PM | |
Joined: 11/5/2018 Last visit: 9/12/2024 Posts: 4 Rating: (0) |
Hello! Initially, the project was completed in WINCC 6.0 SP3, then converted to WinCC 7.0. The next step was converted to WinCC 7.4 SP1 Upd 8. The server project is running Windows Server 2008, and the client projects are on Windows7. At the same time, there are no comments to the server project, but the client project when starting graphic design is given an "out of memoty" error and hangup occurs. How to deal with it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/28/2019 1:25:24 PMNew subject after splitting |
|
3/31/2019 11:51 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41)
|
Hi, in this case I would recommend to create a service request and send the SDT data to the technical support: https://support.industry.siemens.com/cs/ww/en/sc/2090 Regards |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on