4/8/2019 3:21 PM | |
Posts: 1 Rating: (0) |
I have problem with module F-DI 8x24VDC HF (6ES7 136-6BA00-0CA0). I recevie ifnormation as below and I don't know what is the reason of the problem. I think that I checked everything and now I don't have more idea how can I solve it. "Check the PROFIBUS DP/PROFINET IO connection and ensure that there are no external sources of interference. Check the F-monitoring time of the F-IO in the hardware and network editor." Rest of the mofules F-DI 8x24VDC HF are ok. [snip] ------------------------------------------------------------------------------------------ |
Last edited by: BabuMoshai at: 4/8/2019 8:52:35 PMLast edited by: Jen_Moderator at: 4/9/2019 9:12:07 AMRemoved links, because they are not safe and prohibited. Last edited by: Jen_Moderator at: 4/9/2019 9:13:16 AMNew subject after splitting |
|
12/19/2019 2:27 AM | |
Posts: 1 Rating: (0) |
Hello , i got the same problem like you , have fix it? And how? Thanks a lot. My system is ET200SP-CPU with a F-DI after the head moudle. i'm using TIA V15
|
Follow us on