4/4/2019 6:34 AM | |
Posts: 5 Rating: (0) |
I came to know that SIMATIC S7 is used for S7-series PLCs. But i want to know, why specifically number 7 is used to identify the PLC series? |
4/4/2019 6:56 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
The first PLC from Siemens, the SIMATIC S3 came in 1973, the SIMATIC S5 in 1979 and the SIMATIC S7 in 1994 (found on https://de.wikipedia.org/wiki/Simatic ) The numbers have no technical reason, it's marketing. |
|
|
This contribution was helpful to1 thankful Users |
4/6/2019 10:51 PM | |
Joined: 9/14/2009 Last visit: 12/7/2023 Posts: 41 Rating: (0) |
S3 S5 S7 TIA why not called S9 ? |
4/8/2019 4:26 AM | |
Joined: 10/7/2005 Last visit: 9/19/2024 Posts: 3021 Rating: (1054)
|
Rumors have it that Siemens will first need to persuade Audi to give up their trademark on S9 |
Cheers |
|
This contribution was helpful to3 thankful Users |
4/12/2019 7:51 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi Kalaii, S7 is advanced version than S5. [It is Windows based.] Like version, 5 is advanced to 7. Exact reason is not known!! But "What is there in a name?" |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on