4/12/2019 9:49 PM | |
Posts: 24 Rating: (0) |
Our customer has a system with 3 drives working with absolute motor encoders. They want to install an absolute linear encoder for each drive. I´m trying to configure a DDS0 (existing) for motor encoder and DDS1 (new) for linear encoder. The positioning commands come from a PLC by Profibus DP, so I want to keep the scale, if possible. The linear encoder is BTL7-S512BM5550-P-S115, 24bits, Gray code, resolution 5 µm, range 5550mm, output SSI, conector M12 8 poles. Attached my Scout configuration for linear encoder, mechanics of working motor encoder and mechanics of new linear encoder. It seems to be a wrong configuration, because it doesn´t work propperly. I do not understand all the concepts involved in mechanical configuration. Can you explain, please? Thank you. AttachmentFiles.zip (190 Downloads) |
Last edited by: fredito at: 4/12/2019 9:49:59 PM |
|
4/15/2019 2:11 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, in first example 28000 LU = 1 load revolution in the second example 10000 LU = 10 mm. The relationship between load revolution and distance must fit. 8.8.2 Position actual value conditioning 8.8.2.2 Description https://support.industry.siemens.com/cs/ww/en/view/109763287 Figure 8-6 Actual position value sensing with rotary encoders Figure 8-7 Actual position value sensing with linear encoders |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on