4/18/2019 4:08 PM | |
Posts: 3 Rating: (0) |
Hello I have a question about events in wincc V7.4. I would like to have message in Runtime like event When i press button. In this message i want read: who is logged in to HMI declared in the user administration + the action that executed (click button) Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: ISLA at: 4/18/2019 4:09:27 PMLast edited by: Jen_Moderator at: 4/19/2019 9:52:20 PMNew subject after splitting |
|
4/21/2019 10:47 PM | |
Joined: 9/19/2009 Last visit: 5/5/2024 Posts: 458 Rating: (81) |
Hi You can build your own Alarm with VBScript and Runtime. Please search in User Manual VBScript and you will find a sample. Right know I don´t remember the exact procedure. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/22/2019 11:19 AM | |
Posts: 3 Rating: (0) |
Thanks PHS |
4/22/2019 11:48 AM | |
Joined: 9/19/2009 Last visit: 5/5/2024 Posts: 458 Rating: (81) |
This is the sample: In the following example, the message with the alarm number "1" configured in the Alarm
Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on