3/28/2013 10:01 AM | |
Joined: 10/26/2011 Last visit: 3/18/2024 Posts: 763 Rating: (189)
|
Hello Nithin, I heard from this problem three till four times. It seems, that it is a problem. I think, a Service Request (SR)is known at the PCS 7 hotline. Please create also anownservice request. A lot of reported service requests accelerate the time tosolve it. And you have some additional advantages: If the problem is solved, then you get the solution directly(or you will get it afterthe problem is located). You can create the SR via phone or online entry: https://support.automation.siemens.com/WW/llisapi.dll?aktprim=99&lang=en&referer=%2fWW%2f&func=cslib.csinfo2&siteid=csius&extranet=standard&viewreg=WW&groupid=4000002 Under "Ask the Siemens expert" click on Support Request (mhhh, I thought it called Service Request ). Please tell us, if you get the solution. Thanx. |
SIMATIC PCS 7 - Overview |
|
4/14/2015 2:49 PM | |
Joined: 11/16/2012 Last visit: 2/6/2024 Posts: 227 Rating: (31) |
Hi, I think the behavior is caused by server prefixes required for the call-up path for interlock / permit faceplates. Try this: Warning: Regards |
This contribution was helpful to1 thankful Users |
Follow us on