4/24/2019 12:20 PM | |
Joined: 10/26/2011 Last visit: 5/14/2024 Posts: 761 Rating: (190)
|
Hello, Control Module Types (CMT) and Control Modules (CM) are independent from Advanced ES (AdvES), Process Automation Accelerator (PAA) or Comos. You can use the CM and CMT technology without these software. The only reqirement is the Library Advanced Process Library (APL) that is part of PCS 7. If you have the licences for PCS 7, you can use CMT / CM without additional license. As mentioned above, you also don't nee the software PAA, AdvES and COMOS. "In the CMTs of this library some blocks are marked as Optional." A very good documentation is the Application Example On this entry page you will find not only the documentation but also the BCM library. In the BCM (Basic Control Modules) library you find the BCMs that are standardized and tested technical solutions. In the section "Further information" you will find more useful links to manuals and application examples.
|
Last edited by: Thunderstorm at: 4/24/2019 1:05:01 PMLast edited by: Thunderstorm at: 04/24/2019 13:23:10Last edited by: Thunderstorm at: 04/24/2019 13:23:44Last edited by: Thunderstorm at: 04/24/2019 13:29:37SIMATIC PCS 7 - Overview |
|
This contribution was helpful to2 thankful Users |
4/24/2019 8:44 PM | |
Joined: 2/20/2015 Last visit: 5/23/2022 Posts: 12 Rating: (0) |
Hello Stephan, that was excatly the information I needed. Thank you! |
Follow us on