4/24/2019 1:30 PM | |
Joined: 7/14/2017 Last visit: 4/4/2022 Posts: 33 Rating: (0) |
Hello! I have configured my IoT2040 with Huawei 709S-2 following the steps of this tutorial. I have installed correctly and now I am connected to Internet with the SIM card. Now I want to connect with the IoT2040 remotely. It exists any way to configure the ppp0 IP for that? When I run the command ifconfig I receive this information: ppp0 Link encap:Point-to-Point Protocol inet addr:100.68.136.111 P-t-P:10.64.64.64 Mask:255.255.255.255 UP POINTOPOINT RUNNING NOARP MULTICAST MTU:1500 Metric:1 RX packets:38369 errors:0 dropped:0 overruns:0 frame:0 TX packets:48189 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:3 RX bytes:7771616 (7.4 MiB) TX bytes:19736015 (18.8 MiB) Can I configure something to access to the port 100.68.136.111 remotely? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/25/2019 09:48:35New subject after splitting |
|
Follow us on