4/24/2019 7:41 PM | |
Joined: 7/3/2017 Last visit: 12/12/2023 Posts: 9 Rating: (0) |
Hello . I have built a project to set three inverters all together or separately with a 0-10 Volt voltage. I would like someone to check if it is correct because it is the first time I do analogue.Also i would like to ask if it is right to connect in position 7-8 of the inverterhttp://download.lenze.com/TD/8200-8210-8220-8240__Inverter__v1-0__EN.pdf the M1-U1.sorry for my english is from translation
Attachmentlatomio 2.zip (256 Downloads) |
Last edited by: garis at: 04/24/2019 19:53:59 |
|
4/24/2019 7:53 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
Something is wrong with the ZIP archive. It contains no file (s). |
4/24/2019 8:39 PM | |
Joined: 7/3/2017 Last visit: 12/12/2023 Posts: 9 Rating: (0) |
sorrry ixo. yes i mean terminal 7 and 8 to M1-U1 of the logo. Chapter 4 page 40-41 |
4/24/2019 9:18 PM | |
Joined: 7/3/2017 Last visit: 12/12/2023 Posts: 9 Rating: (0) |
Thank you |
This contribution was helpful to1 thankful Users |
5/1/2019 10:23 AM | |
Joined: 7/3/2017 Last visit: 12/12/2023 Posts: 9 Rating: (0) |
Yes peterakosI'm from Greece you understand it from my English ? |
Follow us on