4/25/2019 1:34 PM | |
Posts: 9 Rating: (0) |
Here is the attachment: Thank you in advance. Best Regards, |
4/25/2019 1:52 PM | |
Posts: 9 Rating: (0) |
Here is the output. Well hopefully, I will get to eventually use it. Thank you again. |
4/25/2019 3:06 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Ok, git isn't installed. That's weird because when I wrote my post it was possible to do the command ./configure. Today with exactly the same commands it fails, because there is no configure script I am trying these commands right now:
This is described here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
4/26/2019 3:14 PM | |
Posts: 9 Rating: (0) |
Thnk you alot. All worked out |
This contribution was helpful to1 thankful Users |
5/23/2019 1:07 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, try the commands from bergmanu above! BR |
Follow us on