4/26/2019 12:56 PM | |
Posts: 10 Rating: (0) |
Hello everyone, I want to Connect a PC Station to an S7-1200 using OPC, so I create the project in TIA-Portal v15.1 using the description application : https://cache.industry.siemens.com/dl/files/679/39960679/att_117996/v3/39960679_s7-1200_opc_simatic-net_tia-portal_e.pdf Everything went ok, until I try to download the project to PC Station. I get the error : " loading will not be performed because preconditions are not met " and as an action " load Station manager " (please check a screenshot attached): thank you for helping me |
4/26/2019 2:24 PM | |
Posts: 10 Rating: (0) |
Hello Christoph, Thank you for your answer, to be honest , I don't get what you mean. Please find attached a screenshot of the configuration of "station configuration editor" , thank you to confirm if it is what you mean, otherwise I will be grateful if you give me more detail. AttachmentCapture1.pdf (171 Downloads) |
4/26/2019 2:49 PM | |
Posts: 10 Rating: (0) |
Hello, Yes, as you can see in the attached document, I made the configuration by exporting the xdb file. AttachmentCapture2.pdf (143 Downloads) |
4/26/2019 3:08 PM | |
Posts: 10 Rating: (0) |
Hello, it's in the third indexe, as shown in the sreenshot. AttachmentCapture3.pdf (157 Downloads) |
4/29/2019 1:48 PM | |
Posts: 10 Rating: (0) |
Hello Christoph, do you have an idea what could cause this error besides the order of the indexes ? Thank you for your help. |
4/29/2019 2:13 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, at the mopment no. Which simatic net version is installed? Regards Christoph |
4/29/2019 2:23 PM | |
Posts: 10 Rating: (0) |
Hello, it is the version 15.0 Best regards |
This contribution was helpful to1 thankful Users |
Follow us on