1/25/2018 3:20 PM | |
Posts: 18 Rating: (0) |
Hi guys I try to connect to 319 3pn/dp but after I have power on the plc, all status leds are on. IT is normal or IT is damage? See the attach photo. Thx in advance ! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/25/2018 3:40:05 PMNew subject after splitting |
|
1/25/2018 3:43 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
Hello, it is damage. Regards Christoph |
1/25/2018 3:44 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello Paulo; Fron your attached picture we can see you have no MicroMemory Card (MMC) slotted in the CPU. Do you have ccess to a MMC for this CPU? Such a MMC is required for the CPU to operate, it acts as Load Memory for the PLC: this is where programs and configuration data from your programming software is copied when you download to the CPU. For more infrmation on the MMC as Load memory, please open the following link: MMC as Load Memory for S7-300 CPUs For MMC part numbers for your particular PLC check the file attached to this FAQ document: Which memory cards can you use with an S7-300 CPU? The attached picture below illustrates the points discussed. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/25/2018 3:59:04 PMLast edited by: Jen_Moderator at: 1/26/2018 6:37:54 AMInserted right link. |
|
1/25/2018 4:13 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
the PLC is damaged |
1/25/2018 4:51 PM | |
Posts: 18 Rating: (0) |
Ok,thx Any ideea what I have to check inside the plc on pcb? I am an electronist. |
1/25/2018 5:12 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello Paulo; Some entries in the following discussion could be of help in your situation: cpu-319-not-responding-all-led-are-on-constantly Hope this helps, Daniel chartier |
1/26/2018 1:13 AM | |
Joined: 10/25/2016 Last visit: 9/1/2022 Posts: 199 Rating: (25) |
Hi, You can try to update the firmware. https://support.industry.siemens.com/cs/fr/en/view/23992548 Regards |
Last edited by: Jen_Moderator at: 1/26/2018 6:38:58 AMInserted right link. |
|
Follow us on