4/30/2019 1:50 PM | |
Joined: 3/14/2010 Last visit: 4/14/2024 Posts: 359 Rating: (5) |
Thank you all for your reply and for information ! But I don't needed too much. That was enough for me https://support.industry.siemns.escom/c/ru/ru/view/109758223/en It works Ok. To trace the essential buttons (such as "Go to Warning & Alarm Setpoints Screen" e.g.) I use some system funtions from "Function List". I create an internal WORD and assign every its bit to a certain essential button. I configure a button so that when a button is pressed the bit in the WORD is set, when the button is realesed the bit is reset. Thus I get the changing bits in the WORD and then the word is used in the Alarm System as "Discrete Alarms" but based on internal bits.
|
Last edited by: Alex3110 at: 04/30/2019 13:53:14Last edited by: Alex3110 at: 04/30/2019 19:44:59Last edited by: Alex3110 at: 04/30/2019 19:48:17Last edited by: Alex3110 at: 04/30/2019 20:15:39 |
|
Follow us on