5/6/2019 5:22 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi If you want to use "Dynamic Dialog" and you have a complex task , you can build a function and call this function from Dynamic Dialog Dynamic Dialog = ANSI C Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/7/2019 3:23 PM | |
Posts: 165 Rating: (2) |
Can I make the function in VBS? |
5/7/2019 3:43 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi No, you can´t. Has to be with ANSI C, so translate your function to ANSI C. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on