5/6/2019 5:39 PM | |
Joined: 1/29/2019 Last visit: 7/31/2024 Posts: 27 Rating: (0) |
Hello, I am commissioning a 5 axis machine with RTCP and safety integrated. TRAORI works fine. But while executing cycle 800 I am getting an error. " 17020 illegal array index 1. what can be the reason? if you check HELP it says that related with the parameter number 18077 but I tried to change it still error remains same. in help remedy, it suggested that "IF AN SPL USED IN SAFETY INTEGRATED, THE FIELD INDEX VIA OPTIONAL DATA MAY BE SUBJECT TO ADDITIONAL RESTRICTION". But i really not understand this statement. i am using An SPL So how I can avoid this error? i have attached the screenshots AttachmentCYCLE 800.zip (69 Downloads) |
5/7/2019 8:32 AM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating: (77) |
$MC_TRAFO5_TCARR_NR_x = <TCARRNR> $MC_TRAFO_TYPE_x = 72 and related parameters (e.g. CHAN axes) |
hope that helps |
|
5/7/2019 9:00 AM | |
Joined: 1/29/2019 Last visit: 7/31/2024 Posts: 27 Rating: (0) |
I have tried to set 24582 but still gives the same alarm. and my TRAFO TYPE is 24 I have attached my NC.arc. can you please have look. I really can't get where I made a mistake AttachmentNC.txt (80 Downloads) |
5/7/2019 1:59 PM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating: (77) |
three modified data |
hope that helps |
|
5/8/2019 1:35 PM | |
Joined: 1/29/2019 Last visit: 7/31/2024 Posts: 27 Rating: (0) |
after changing 28082 to 3D .its working fine even with TRAORI type 24 |
Follow us on