4/29/2019 9:29 AM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating: (69) |
Hello Prattsega, I think now I understand want you want to do. You need a text input/output field, which you can edit with a click on it. Then the keyboard should come up and after you're finished with the text input, the text should be displayed at the output field. Am I correct? My suggestion:
Setting focus may be set by the following code, wich I got from this topic: https://support.industry.siemens.com/tf/ww/en/posts/focus-on-i-o-field/115594?page=0&pageSize=10 Dim IOFIELD Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
This contribution was helpful to1 thankful Users |
5/3/2019 6:55 AM | |
Posts: 21 Rating: (0) |
Hi Nzett11, You almost understood me , just the thing is that instead of text i want to enter numeric value in the selected Input field. So its like text input /output field but the text of the button or the I/O Field is constant. and on click the keyboard opens and when i enter numeric value then it should stored in other some tag. Let me know if you find any other ways. Because, in previous solution i need to move focus on some input field. but i dont have any input field on that page also input field do not have invisible property. so not working for me. Attachmentsiemens button numpad..pdf (103 Downloads) |
Follow us on