4/27/2019 2:28 AM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
I installed pcs7 v9 sp1 on windows server 2016 and error 2772:105 in wizard creating os bjects And installed on windows server 2012r2 [pcs7 engineering +os single station ]then error 2772:105 Please help On laptop and pc tested “I don’t see any thing of sql server 2014 in stat menu!!!!” And I separate install from directory pcs7 AttachmentNew folder (2).zip (240 Downloads) |
Last edited by: PLC2011 at: 04/27/2019 12:09:30 |
|
4/28/2019 11:51 AM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
i think this problem i see in setup menu of pcs7 v9 sql server2014 and i dont see sql server 2014 in install menu of pcs7 v9 sp1 what occuor this problem? i no problem with V9 my problem is V9SP1 AttachmentNew folder.zip (265 Downloads) |
Follow us on