5/11/2019 10:39 AM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Hi Plese, can you explain a litle more about this task. Do you want execute an App inside WinCC? Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/11/2019 9:15 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684) |
Hello Rafal; I believe that it is no linger possible to run WinCC over Windows Embedded. The supported OS list does not show this possibility anymore (see the attachment below) https://support.industry.siemens.com/cs/ww/en/view/109736216. At one point, Siemens decided to provide one of its model of industial PCs (IPC427C) with a WinCC "bundle" (special package) running with Windows Embedded 2009. This installation was limited to this particular hardware and software ennvironment. The WinCC package came on a spêcial memory card that was to be inserted in the IPC and run from the memory card. So I cannot see how it could be installed with an OMRON machine. In any case, Siemens opted to remove this option on subsequent offers of WinCC, and today you can only purchase standard OS-based versions of WinCC. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 05/11/2019 21:17:46 |
|
Follow us on