5/13/2019 9:23 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hello, After a few weeks of the attached program running, a small problem has come to light. the machine stop part of the program has a count for number of stops and a timer made up of hours, minutes and seconds recording the elapsed time. Although the machine stop part of the program works flawlessly in a logo simulation offline.In a running and live state the actual number of stops does not increment singularly for example I4 is activated and the counter displays 4 as the number of stops whilst the machine has only stopped once and if the machine is stopped for a second time the counter could display 10 it seems purely random.But the counter works fine during a offline simulation. at this moment in time i am totally baffled, so i would be grateful for some pointers in clearing this matter up Ade AttachmentInverter_Speed_Preset_ACM2_v3.1_Gain1.0.zip (119 Downloads) |
5/13/2019 10:06 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
LOGO BM 24 RCE:- 6ED 1052-1HB00-0BA8 |
5/13/2019 10:11 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32847 Rating: (4061)
|
This LOGO! has no fast count inputs. Then must the On-/Off Delay solve your problem, I think. |
Follow us on