5/13/2019 9:45 AM | |
Joined: 6/1/2017 Last visit: 5/8/2024 Posts: 13 Rating: (0) |
Hi everyone ! I have a program in STL language having many analog module BUt problem is that Piw & PQW not used in program and every analog input & output is working good on machine. PIW , IW ,PQW & QW can replaced any other address or syntex. I have seached in cross refernce per. inut & output but nothing show . please see the attachments ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/13/2019 14:31:52New subject after splitting |
|
5/13/2019 8:12 PM | |
Joined: 6/1/2017 Last visit: 5/8/2024 Posts: 13 Rating: (0) |
Any syntex of which is use without piw & pqw |
5/13/2019 10:09 PM | |
Joined: 9/21/2012 Last visit: 9/19/2024 Posts: 4147 Rating: (464) |
For example, a blcok that is used in the code, that has an input called LADDR. |
5/15/2019 6:50 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Can't find any PIW & PQW is published within the conference STEP 7 / STEP 7 Lite. Best regards Jen_Moderator |
Follow us on