5/7/2019 4:25 AM | |
Joined: 4/24/2019 Last visit: 6/21/2022 Posts: 1 Rating: (0) |
Dear Experts, I have one question regarding SE PO upgrade for CPU 410H. 1. Will the CPU stop during the PO activation? Thank you so much.. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/07/2019 06:51:01New subject after splitting |
|
5/7/2019 9:15 AM | |
Joined: 8/1/2017 Last visit: 3/18/2024 Posts: 14 Rating: (17) |
Hello yangyan666, the answer to your question can be found in this topic: The short answer to your question is, no it will not stop the CPU during the license upgrade. Best regards, Stephan
|
This contribution was helpful to2 thankful Users |
5/7/2019 10:12 AM | |
Joined: 11/10/2010 Last visit: 3/5/2024 Posts: 165 Rating: (8) |
Dear yangyan666, no the CPU will not stop during the PO upgrade and activation.
|
5/15/2019 11:04 AM | |
Posts: 36 Rating: (1) |
Hello , For online PO upgrade withut CPU Stop you need , below the requirement : - SIMATIC PCS 7 V8.1 or higher - CPU 410-5H firmware V8.1 or higher - The CPU 410-5H is configured with firmware V8.1 or higher in the HW Config - The SEC of the CPU 410-5H has the product version 2 or higher
|
This contribution was helpful to2 thankful Users |
Follow us on