5/16/2019 10:23 AM | |
Joined: 2/20/2019 Last visit: 4/23/2024 Posts: 2 Rating: (0) |
I have two devices in an industrial factory, where they have their own network, and through the VPN I have access to them, but they use a firewall. Devices: PLC S7-1500 & a HMI KTP700 panel. In the case of the PLC, they open Port 102 and with TIA Portal I am able to establish an online connection and make modifications. However, with the HMI panel, they open Port 2308 but I can neither communicate with it nor transfer modifications. According the the information I have obtained from the following link: https://support.industry.siemens.com/cs/ww/en/view/24534065 the problem is that their end must enable a port range (from 1024 to 65534) for me to be able to communicate with, and transfer to, the HMI panel. Does there exist any other way to do this, or am I mistaken, and the panel’s dynamic communication port can be changed to static using Microsoft Windows or TIA Portal’s configuration options? This way, the factory where I have the devices would be able to reserve the ports that I strictly need. Thank you. I hope to receive answers. |
Last edited by: Jen_Moderator at: 05/16/2019 14:31:07Optimized link. |
|
5/27/2019 3:02 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello ivancanet no there is not used a Port Range in TIA Portal any more. if you look in the TIA Portal Help System then you will see that you need only: https://support.industry.siemens.com/cs/de/en/view/109755202/105572859275 1033, 2308, 50523 -> you should not need in the "Extended Download to Device" dialog the Option "Show all compatible devices". Use instead "Show devices with the same addresses" or you type the IP Adress manually in the Table. Its because the DCP Packages will not come through the VPN Router. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on