5/16/2019 11:06 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello rogerdc; Have a look at the following document: SICAM P850/P855 - 7KG85 - Power Monitoring Device and Power Quality Recorder - Device Manual https://support.industry.siemens.com/cs/ww/en/view/109752151 The standard access to parameters of the power meter is through a web browser. The only discussion of CID files appears when the P850 is used along with SICAM PQS, to store and archive power meter data for reports and exports. See chapter 3 in this document: SICAM P850/P855 - 7KG85 - Power Monitoring Device and Power Quality Recorder - System Manual https://support.industry.siemens.com/cs/ww/en/view/109752152 Hope this helps, Daniel Chartier |
5/17/2019 2:50 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello rogerdc; SICAM products are part of a portfolio of products developed and distributed by Siemens Energy. This division is sepperate from the Siemens IA&D division that supports this forum. We have access to some documentation of the P850 power meter units, since we may use them in some of our projects, but what I have provided as documentation is at the limit of our potential help. The first manual link provided earlier contains a description of the IEC 61850 server communication mesurands available for the P850. This does not describe the IEC 61850 client application needed on your RTU, using PMDIF or COMTRADE files. The second manual link discusses the possible use of PQS software to connect the data from the P850 to additional software. I have no further information at this time that I can provode. One of our members, Mike J, has links to Siemens Energy and great experience with their products, you might want to search for his posts on SICAM products on this forum: https://support.industry.siemens.com/tf/ww/en/users/profile/14688/
Hope this helps, Daniel Chartier |
Follow us on