4/25/2019 7:14 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (267) |
Hello arunvt1992, Let me give you my takes: 1. Screenshots all the screens in HMI as much as you can, all parameters, all equipments. This is to prevent any unforseen situations happened after the full download. May be a valves suddenly claimed that no communication after download? then you can show them the proof saying that the valves were no communication before the download. These goes to all parameters including the process mode. 2. Do a readback in all CPU you have. Chart-> Readback. For safety PLC, be-mindful. Sometimes I prefer to leave the Safety PLC in its original state instead of readback version. 3. you can do a hardware configuration Online Screenshot if you want. 4. Do an Archive before Readback, after readback. 5. If you wanna update some function blocks/ library, do now. 6. Full Compile 7. Full Download. 8. Compare and check everything again. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
5/18/2019 10:56 AM | |
Joined: 10/5/2016 Last visit: 4/17/2024 Posts: 85 Rating: (0) |
Thanks a lot Jaztai and Martin... I will insert in new OB . |
Follow us on