5/17/2019 2:53 PM | |
Joined: 10/14/2009 Last visit: 10/17/2022 Posts: 140 Rating: (1) |
Hello Iam new in simotion. I have system of SIMOTION 445-2 " with CF card" controlling 3 servo motors and there are 5 sinamics 3 phase drives controlling usual motors all communicated using p. After the machine power on in this morning I found SF led on at the Simotion "see attached" I used service siwitch to retain diagnostic buffer on CF but no success to read I used service switch 'PLC" by move it from 0 to 1 then to 0 again to reset the simotion but no success to eleinate SF My questions 1- How to see SIMOTION diagnostic buffer to clear SF reason....I tried to go online and succed to find the simotion but can not find the buffer 2- there a message one one of the 3ph drives "Fault T5 F6310" after check the manual found that related to supply voltage ......then check and the supply is 380 v and r208 is 400 v 3- Seven segment in SIMOTION is "6" what does this number mean?all AttachmentDoc1.pdf (283 Downloads) |
5/18/2019 1:42 PM | |
Joined: 10/14/2009 Last visit: 10/17/2022 Posts: 140 Rating: (1) |
Hello Do you mean S7 or Simatic manager ?!!! |
5/18/2019 6:23 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980)
|
Hi, step7 or simatic manager, where is the difference? You can use both for the diagnostic.
Christoph |
Follow us on